AXIS#.WS.ARM

Description

This command sets wake and shake to start at the next axis enable. Feedback type is not relevant for this command. If AXIS#.WS.STATE is 0 and the drive is disabled, then AXIS#.WS.STATE will change to 1 after issuing AXIS#.WS.ARM. With this command, wake and shake can be repeated if desired.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.WS.ARM

5013h

09h

Unsigned32

-

-

Write only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6700

1

6700 (0x1a2c)

AXIS1.WS.ARM

Unsigned8

Read/Write

No

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.WS.ARM

6700

Unsigned8

Read/Write

-